Read (FB; Prefix filrd)
FUNCTION_BLOCK Read EXTENDS CBM.ETrigToA
szBuffer”,
the function block returns an active ”xDone” and indicates the current number of characters in ”szSize”. The size of the target memory structure
for the bytes to be read and the number of bytes to be read will not be checked.- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrigToA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigToA
udiTimeOutUDINTDefines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.
ETrigToA
Output
xDoneBOOLTRUE: Action successfully completedETrigToA
xBusyBOOLTRUE: Function block activeETrigToA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigToA
xAbortedBOOLTRUE: Action aborted by userETrigToA
Input
hFileCAA.HANDLEFile handle
pBufferCAA.PVOIDTarget address for the first byte to be read; can be retrieved via operator ADR
szBufferCAA.SIZEMaximum number of bytes to be read; can be retrieved via operator sizeof
Output
eErrorLocal library error ID (0: no error; 5101: time out)
szSizeCAA.SIZECurrent number of successfully read bytes; this value is already valid before
xDonehas been set