GetTransmitErrorCounter (FUN)
FUNCTION GetTransmitErrorCounter : CAA.COUNT
Returns a counter which is incremented with each transmit error. Diagnostic Information can be also read by GetDiagnosis.
- InOut:
Scope
Name
Type
Comment
Return
GetTransmitErrorCounterCAA.COUNTnumber of transmit errors
Input
hDriverCAA.HANDLEhandle of CAN interface
peErrorPOINTER TO ERROR
optional pointer to error enum