GetBusload (FUN)
FUNCTION GetBusload : USINT
This function is not implemented by all drivers. It returns the current busload in percent. Diagnostic Information can be also read by GetDiagnosis.
- InOut:
Scope
Name
Type
Comment
Return
GetBusloadUSINTbus load (0..100) in percent
Input
hDriverCAA.HANDLEhandle of CAN interface
peErrorPOINTER TO ERROR
optional pointer to error enum