AlarmStorageReader.prvRetrieveLatchVarValue (METH)
METHOD prvRetrieveLatchVarValue : STO.ERROR
Reads the value of a latch variable from the alarm storage and stores it in the passed IAlarmMetaObjectStub3 instance.
- InOut:
Scope
Name
Type
Comment
Return
prvRetrieveLatchVarValueSTO.ERROR- A STO.ERROR value indicating the success or failure of the operation:
NO_ERROR: In case of success
WRONG_PARAMETER: If
iWhichLatchVarreferences to an invalid latch variable
Input
itfDatabaseAccessIDatabaseAccessThe instance of IDatabaseAccess, that is used to access the database
itfAlarmMetaObjectStub3IAlarmMetaObjectStub3An instance of IAlarmMetaObjectStub3, where the values will be stored
usiWhichLatchVarUSINTThe 1-based index of the latch variable.