AlarmStorageReader.Read (METH)
METHOD Read : EAlarmStorageReaderErrors
Reads data from the alarm storage.
- InOut:
Scope
Name
Type
Comment
Return
Read- A EAlarmStorageReaderErrors value indicating, whether the processing has been completed successfully or not:
EAlarmStorageReaderErrors.NoError: Completed successfully
EAlarmStorageReaderErrors.WrongParameter: If the IAlarmStorageReaderConsumer instance is invalid
- EAlarmStorageReaderErrors.AdditionalReadCallRequired: Reading has been completed successfully, but there is
additional call of method ContinueReading necessary to read the rest of the data
Input
liTimstampFromLINTThe timestamp (when the alarm became active) of the 1st alarm
liTimstampToLINTThe timestamp of the last alarm
xReadAscendingBOOLIf this parameter is TRUE, then the rows will be returned by “timestamp active” ascending, otherwise descending
itfAlarmStorageReaderConsumerAn instance of IAlarmStorageReaderConsumer, to which the data read from the alarm storage will be passed.