AlarmStorageGetTextListName (FUN)

FUNCTION AlarmStorageGetTextListName : POINTER TO STRING

This function can be used to determine the name of the textlist of an alarm group, that was read from the alarm storage.

InOut:

Scope

Name

Type

Comment

Return

AlarmStorageGetTextListName

POINTER TO STRING

A pointer to a STRING containing the name of the textlist. A NULL pointer if the corresponding information cannot be retrieved

Input

udiAlarmGroupId

UDINT

The internal id of the alarm group, that was read from the alarm storage