Alarm Manager Internal Interfaces (LIB)

Version

4.8.0.0

Namespace

AlarmManagerInternal_Interfaces

Author

CODESYS Development GmbH

Description 1

This library defines the internal interfaces of the alarm management, that are used by the alarm table and the alarm banner

Contents:

Indices and tables

1
Based on AlarmManagerInternal_Itfs.library, last modified 17.04.2025, 08:19:50. LibDoc 4.6.0.0-r.29
The content file AlarmManagerInternal_Itfs.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 17.04.2025, 08:19:52.