MqttConnectWithCertStore (FB)
FUNCTION_BLOCK MqttConnectWithCertStore EXTENDS AbbETrig3
Establish a Connection to the MQTT broker using a certificate from the Certificate Store
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
ExecuteBOOLFALSE
A rising edge starts a single operation, the output Busy goes to TRUE. In the first cycle all other inputs are read and stored, afterwards they are ignored. A falling edge does not stop the operation. After Done = TRUE or Error = TRUE and Execute = FALSE all outputs will be reset. For executing another operation the Execute input needs to be retriggered by another rising edge!
AbbETrig3
Output
DoneBOOLFALSE
Operation is completed without error (while outputs Busy and Error are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE
AbbETrig3
BusyBOOLFALSE
Operation is running (while outputs Done and Error are FALSE)
AbbETrig3
ErrorBOOLFALSE
Operation is stopped with error (while outputs Busy and Done are FALSE). This output is TRUE for at least one cycle or until Execute is set to FALSE. The output ErrorID gives more details about the error.
AbbETrig3
Input
ConnPOINTER TO MQTT_CONNECTION
0
Pointer to empty / uninitialized MqttConnection struct. Upon successful completion of this FB, this struct can be used to operate all other MQTT FBs.
IpAddressSTRING(Constants.MQTT_MAX_IP_ADDRESS_LEN)Defaults.MQTT_DEFAULT_EMPTY
IP address of the MQTT Broker.
PortWORDDefaults.MQTT_DEFAULT_PORT
Port number of the MQTT Broker.
SecureBOOLDefaults.MQTT_DEFAULT_SECURE
True = Use secure channel for communication (TLS).
ServerCertSTRING(Constants.MQTT_SHA1_LEN)Defaults.MQTT_DEFAULT_EMPTY
Server certificate thumbprint from store. (SHA1 in hex chars like ‘dd454bfc704d844b8d2cbe729fcfb8ed2d2e3f6a’)
ClientCertBOOLDefaults.MQTT_DEFAULT_CLIENTCERT
True = Use Client certificate from store.
ClientIdSTRING(Constants.MQTT_MAX_CLIENT_ID_LEN)Defaults.MQTT_DEFAULT_EMPTY
Client Identifier used to identify the client and the related session.
UsernameSTRING(Constants.MQTT_MAX_USERNAME_LEN)Defaults.MQTT_DEFAULT_EMPTY
Username of a user used by the MQTT Broker.
PasswordSTRING(Constants.MQTT_MAX_PASSWORD_LEN)Defaults.MQTT_DEFAULT_EMPTY
Password for this user.
LastWillOptional Last Will message.
KeepAliveWORDDefaults.MQTT_DEFAULT_KEEPALIVE
Time in seconds, which will be passed to the MQTT Broker and which is normally used by the Broker to disconnect clients if no communication was made for 1,5 * KeepAlive
TimeoutWORDDefaults.MQTT_DEFAULT_TIMEOUT
- Timeout in ms for all network communication of the following Function Blocks: MqttConnectWithCertBuffer,
MqttConnectWithCertFile, MqttConnectWithCertStore, MqttDisconnect, MqttPing, MqttPublish, MqttSubscribe, MqttUnsubscribe. If the FB did not receive any communication for that amount of time it will terminate the execution and return MQTT_ERR_COMMUNICATION_TIMEOUT error.
Output
ErrorIDERROR_ID.MQTT_ERR_NO_ERROR
Error code description