MQTT_CONNECTION (STRUCT)
TYPE MQTT_CONNECTION : STRUCT
strcuture to hold all relevant internal data of an MQTT connection. Will be filled by the MqttConnect* POUs
- InOut:
Name
Type
Comment
abyConnARRAY [0..Constants.MQTT_CLIENT_STRUCT_SIZE] OF BYTE
Internal connection structure
abyTxBufARRAY [0..Constants.MQTT_TX_BUF_SIZE] OF BYTE
Internal send buffer
abyRxBufARRAY [0..Constants.MQTT_RX_BUF_SIZE] OF BYTE
Internal receive buffer
abyMsgBufARRAY [0..Constants.MQTT_MSG_BUF_SIZE] OF BYTE
Internal message buffer for incoming messages