|
This is the web edition of the original ⮫ AC500-S safety user manual, version 1.4.0. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements. |
According to ⮫ [2], annex C.2.
F-Devices that should be shut down due to energy efficiency reasons or for maintenance reasons require an F-Host extension that allows to ignore host timeout/CRC errors.
After the application sets Disable_C = TRUE, the F-Host is requested to use fail-safe values for this F-Device.
Disable_S = TRUE reports the application that the F-Host is now using fail-safe values. Timeout/CRC errors from the F-Device are ignored while Disable_S = TRUE.