Each node in the device tree has a diagnosis view, which displays the diagnosis messages for this device only.
The message consists of the following:
-
Timestamp in date and time YYYY-MM-DD hh:mm:ss.ms
-
Error severity
-
Error code
-
Diagnosis description
-
Additional data
To view the diagnosis message, do as follows:
-
Double-click on a device.
-
Select the tab “Diagnosis”.
Device diagnosis is disabled by default.
To enable/disable device diagnosis:
-
Double-click on the PLC.
-
Select the tab “PLC Settings”.
-
Under “Additional Settings” enable/disable “Diagnosis for devices”.
When the device diganosis is disabled, this symbol
will be displayed in the device tree and no diagnosis messages will be shown.