OverviewPermalink

The declaration editor is used to declare variables of POUs and global variables, for data type declarations, and in the Watch and Receipt Manager. It gives access to the usual Windows functions, and even those of the IntelliMouse can be used if the corresponding driver is installed.

In Overwrite mode, 'OV' is shown in black on the status bar; switching between Overwrite and Insert modes can be accomplished with the <Ins> key.

The declaration of variables is supported by syntax coloring.

⮫ “Syntax coloring”

The most important commands are found in the context menu (right mouse button or <Ctrl>+<F10>).

Consider the possibility of using pragmas to affect the properties of a variable concerning the compilation resp. precompilation process.

⮫ “Pragmas, overview”

⮫ “Declaration part”

⮫ “Input variable”

⮫ “Output variable”

⮫ “Input and output variables”

⮫ “Local variables”

⮫ “Constants, typed literals”

⮫ “External variables”

⮫ “Keywords”

⮫ “Variables declaration”

⮫ “AT Declaration”

⮫ “'Insert' 'Declaration keywords'”

⮫ “'Insert' 'Type'”

⮫ “Syntax coloring”

⮫ “Shortcut mode”

⮫ “Autodeclaration”

⮫ “Line numbers in the declaration editor”

⮫ “Pragma instructions for initialization, monitoring, creation of symbols, bitaccess, linking”

⮫ “Declarations as table”

⮫ “'Insert' 'New declaration'”

⮫ “Declaration editors in online mode”