'Insert' 'New declaration'Permalink

With this command you bring a new variable into the declaration table of the declaration editor. If the present cursor position is located in an field of the table, then the new variable will be pasted in the preceding line; otherwise, the new variable is pasted at the end of the table. Moreover, you can paste a new declaration at the end of the table by using the right arrow key or the tab key in the last field of the table.

⮫ “Declarations as table”

You will receive a variable that has "Name" located in the Name field, and "Bool" located in the Type field, as its default setting. You should change these values to the desired values. Name and type are all that is necessary for a complete declaration of variables.