Symbol: 
Function: This command opens the “Select revision” dialog. In this dialog, you select the revision to which the project or the selected objects revert.
Call:
-
“Project SVN”
-
“Context menu SVN”
If nothing or the base node is marked in the object tree, then the entire project is reverted to a specific revision (“Revert project to revision”). If one or more objects are selected, then these objects and their sub-objects are reverted (“Revert to revision”).
Dialog 'Select revision'
For a description of the dialog, refer to the section "Select revision".