Dialog 'Select revision'Permalink

Function: This dialog shows the currently selected revision. You can edit the selection there.

“Revision”

“HEAD”

_icon_radiobutton_acitvated: The latest revision (top revision) within a branch is displayed.

“Revision”

_icon_radiobutton_acitvated: A specific revision is displayed by the revision number.

Example: ‎3‎

Tip: Click _svn_button_three_dots to show the revisions. Then the “Log” dialog opens to display the revisions and the associated actions. The revision that you select there is applied.

“Date”

_icon_radiobutton_acitvated: A specific revision is checked out by the modification date. This is the highest revision at the given time (the last revision before that time).

Example: ‎12/23/2016 11:59:59‎

Tip: See section "Revision identifiers" in "Version control with Subversion"

“Use UTC Time”:

_cds_icon_option_activated: Modification date in universal time is used.

“Reset recursively”

_cds_icon_option_activated: All objects below the selected object are also reset.

The action fails if

  • Objects have been moved in or out of the hierarchy below

  • Objects outside of the hierarchy would be changed by implicit dependencies

See also