Command 'Revert', Command 'Revert project'Permalink

Symbol: _svn_icon_revert

Function: This command opens the “Revert” dialog. In the dialog, select the objects whose local changes should be reverted, and those that are reverted to the state of the base revision of the working copy.

Call:

  • Menu bar: “Project  SVN”.

  • “Context menu  SVN”

If you select nothing or the main node in the device tree, then all modified objects are listed in this dialog (“Revert project”). If you selected one or more objects, then only the changes to this object are listed and recursively their sub-objects (“Revert”).

Dialog 'Revert'

“Group externals”

_cds_icon_option_activated: The external definitions are grouped by their external storage locations.

“Keep locks”

_cds_icon_option_activated: The lock is retained for all files that are modified by the revert command.

“Select/deselect all”

When external objects are deleted, CODESYS SVN cannot restore this data in SVN offline mode. The user is prompted how to proceed:

  • Switch back to SVN online mode and call the external objects.

  • Connect now to the SVN server one time in order to complete the current operation, but afterwards switch back to SVN offline mode.

  • Skip the retrieval of the external objects. They can be fetched later by updating the project.