Symbol:
Function: The command checks whether or not a text list entry in the project is used as a static text. If this is the case, then the text list entry is removed from the text list.
Call: “Text List” menu; context menu
Requirement: The “GlobalTextList” is open and active. A field is selected in the table.
For more information, see: ⮫ “Using a Text List ”, ⮫ Further information, ⮫ “Localization with static text ”, ⮫ “Output of dynamic text by a variable ”