When you insert a text into a visualization element, an entry is generated in the
GlobalTextList
global text list as a result. GlobalTextList
is automatically generated and supplemented and therefore contains all texts which
are permanently (statically) configured in the visualizations. In particular, when
you insert something into the “Texts → Text” element property, a new entry is automatically created for it in GlobalTextList
.
In GlobalTextList
, you can translate the automatically specified default texts and add more languages
when needed. If language switching is implemented for visualizations, then the translation
from GlobalTextList
is displayed at runtime for the configured text.