Symbol:
Function: The object contains the properties, meta-information, and project information. With this, you can check the authorship and integrity of the project.
Call
-
Double-click the object in the device tree
-
“Project Project Information” menu
Requirement: CODESYS creates the object when you click “Project Project Information”, and the dialog opens.
CODESYS saves the project information directly in the project. For example, when you transfer a project to another system, the “Project Information” object is also transferred. You do not need a project archive.
For more information, see: ⮫ “Retrieving and Editing Project Information ”
-
See also: ⮫ __POOL