Parameters (PARAMS)
- InOut:
Scope
Name
Type
Initial
Comment
Constant
gciNumberOfPositionAxes
INT5
The number of position axes which are used in MCA_CommandTable
gciNumberOfSpeedAxes
INT5
The number of position axes which are used in MCA_CommandTable
gciNumberOfTappets
INT10
The number of tappet points which are used in MCA_CommandTable
gciMaxCommandLines
INT200
The maximum number of commands in MCA_CommandTable