EVTPARAM_CmpRdcyAcyclicRecv (STRUCT)
TYPE EVTPARAM_CmpRdcyAcyclicRecv : STRUCT
- InOut:
Name
Type
Comment
szDataUUIDSTRING(36)IN: Data UUID that was used for sending the data. Note: The size of STRING(36) is 37 bytes.
aFillBytesARRAY [0..2] OF BYTE
3 unused fill bytes for correct alignment of the next element in this struct.
pBufferPOINTER TO BYTE
IN: The pointer to the buffer that contains the received payload data
lengthDWORDIN: The length of the received payload data in bytes