TrendStorageReaderValueConverter.ConvertToLREAL (METH)

METHOD ConvertToLREAL : LREAL

Converts a value read from the trend storage into a LREAL value.

InOut:

Scope

Name

Type

Comment

Return

ConvertToLREAL

LREAL

Input

iWhichVariable

INT

A 0-based index of the variable within all variables, i.e. must be less the parameter iCountVariables of method SetVariableConfiguration

liValue

LINT

The value, that was read from TblTrendData

xValueNULL

BOOL

Indicates, whether NULL is stored in the trend storage

Output

eError

ETrendStorageReaderErrors

Returns a ETrendStorageReaderErrors value indicating, where the processing was completed successfully or not.

  • ETrendStorageReaderErrors.NoError: Completed successfully

  • ETrendStorageReaderErrors.InvalidCall: ConvertToLREAL was called without calling method SetVariableConfiguration before

  • ETrendStorageReaderErrors.WrongParameter: The value of the parameter iWhichVariable is invalid