TrendStorageReader.Read (METH)
METHOD Read : ETrendStorageReaderErrors
Reads data from the trend storage.
- InOut:
Scope
Name
Type
Comment
Return
Read- A ETrendStorageReaderErrors value indicating, whether the processing has been completed successfully or not:
ETrendStorageReaderErrors.NoError: Completed successfully
ETrendStorageReaderErrors.NotInitialized: Call to method Initialize has not been done
ETrendStorageReaderErrors.WrongParameter: If the ITrendStorageReaderConsumer instance is invalid
- ETrendStorageReaderErrors.AdditionalReadCallRequired: Reading has been completed successfully, but there is
additional call of method ContinueReading necessary to read the rest of the data
Input
liTimstampFromLINTThe absolute timestamp of the 1st sample
liTimstampToLINTThe absolute timestamp of the last sample
itfTrendStorageReaderConsumerAn instance of ITrendStorageReaderConsumer, to which the data read from the trend storage will be passed.