VisuFbXYChartGenericVariableArray (FB)
FUNCTION_BLOCK VisuFbXYChartGenericVariableArray EXTENDS VisuFbXYChartGenericVariable
This function block extends VisuFbXYChartGenericVariable. It is used in case of array, like curves.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
pVar__XWORDPoints to the variable
varTypeTypeClassData type of variable
diSizeDINTData size
Methods:
GetValueRAWixUnck
GetValueREALixUnck
CheckVarPointerIsChanged, inherited from VisuFbXYChartGenericVariable
GetValueBOOL, inherited from VisuFbXYChartGenericVariable
GetValueDINT, inherited from VisuFbXYChartGenericVariable
GetValueLREAL, inherited from VisuFbXYChartGenericVariable
GetValueREAL, inherited from VisuFbXYChartGenericVariable
GetValueUDINT, inherited from VisuFbXYChartGenericVariable
GetVariableType, inherited from VisuFbXYChartGenericVariable
SetInitialAddress, inherited from VisuFbXYChartGenericVariable
SetValueDINT, inherited from VisuFbXYChartGenericVariable
SetValueREAL, inherited from VisuFbXYChartGenericVariable
Structure: