VisuFbXYChartGenericVariable (FB)
FUNCTION_BLOCK VisuFbXYChartGenericVariable IMPLEMENTS IXYChartGenericVariable3
This function block is the implementation of the IXYChartGenericVariable interface. It is used by the generated code to provide suitable instances of this interface. It contains parameters to identify a generic variable
- InOut:
Scope
Name
Type
Comment
Input
pVar__XWORDPoints to the variable
varTypeTypeClassData type of variable
diSizeDINTData size
Methods:
CheckVarPointerIsChanged
GetValueBOOL
GetValueREAL
GetValueUDINT
SetInitialAddress
SetValueREAL
GetValueDINT
GetValueLREAL
GetVariableType
SetValueDINT
Structure:
VisuFbXYChartGenericVariable.CheckVarPointerIsChanged(METH)VisuFbXYChartGenericVariable.GetValueBOOL(METH)VisuFbXYChartGenericVariable.GetValueREAL(METH)VisuFbXYChartGenericVariable.GetValueUDINT(METH)IXYChartGenericVariable2IXYChartGenericVariable3VisuFbXYChartGenericVariable.SetInitialAddress(METH)VisuFbXYChartGenericVariable.SetValueREAL(METH)