IRectangleListManager.PushClipping (METH)
METHOD PushClipping
This method intersects the current clipping region used for the rectangles with the given rectangle. Please remark that the given rectangle must not be transformed yet. Of course there must be a matching call to PopClipping Typically the clipping methods are called when necessary in the following order:
- PushClipping // set the clipping rectangle if necessary
PushTransformation // set the transformation for the inner elements
- ForwardCall // forward the rectangle collection to the inner elements
PopTransformation PopClipping
- InOut:
Scope
Name
Type
Input
rectVisuStructSimpleRectangle