IRectangleListManager.ForwardCallWithMouseDownInfo (METH)
METHOD ForwardCallWithMouseDownInfo
- InOut:
Scope
Name
Type
Comment
Input
pElementsPOINTER TO ARRAY [0..0] OF IVisualElement
countINTpMouseDownInfoPOINTER TO ARRAY [0..100] OF BYTE
a pointer to an array of bytes representing a bitfield with the information about elements handling mouse down or not the according bitfield is organized from lower indices to higher indices in general, within single bytes earlier elements are located at less significant bits