VisuFbPaintAfterAllElement.GetCompleteSurroundingRect (METH)
METHOD GetCompleteSurroundingRect : CmpVisuHandler.VisuStructSimpleRectangle
Similar to GetSurroundingRect of IVisualElement. But here, the exact size has to be returned. Means, considering of possible outer frame line widths, which will enlarge the element. As well as considering rotation of the element or acute angles within polygons. Also the returnrect may be different offline or online. As online also dynamic movement is considered. Whereas offline only a possible static rotation can be used.
- InOut:
Scope
Name
Type
Return
GetCompleteSurroundingRectCmpVisuHandler.VisuStructSimpleRectangle