GVL_DebugChecks (GVL)
- Attributes:
qualified_only- InOut:
Name
Type
Comment
IsValidCommandArea
BOOLThis flag marks the valid area from which paintcommands should be added to the paintbuffer. It is for debugging purposes and can be activated with compiler define VISU_CHECK_VALID_PAINTCOMMANDAREA
NumOfPaintCommands
DWORDThe number of paint commands needed for last call. It is for debugging/test purposes and can be activated with compiler define VISU_ASSIGN_NUMOFPAINTCOMMANDS
xStartAddCommand2
BOOLStartAddCommand2 called CanAddCommand -> Indicates if the new improved Cmd is called
NumReleasedClients
DINT