VisuFbBaseVector.InitStaticMemory (METH)
METHOD InitStaticMemory
Utility method that allows initialization of the vectors memory to start with a static buffer if this is supported by the underlying library.
- InOut:
Scope
Name
Type
Comment
Input
pBufferPOINTER TO BYTE
CHECKED_OMIT, not relevant for int. visu and not called at all
udiSizeUDINTCHECKED_OMIT, not relevant for int. visu and not called at all