WebServerFileProtection_Callback.EventCallback (METH)
METHOD EventCallback : CmpEventMgr_Interfaces.RTS_IEC_RESULT
The interface ICmpEventCallback must be registered for an event. If this event is posted, this callback method is called.
- InOut:
Scope
Name
Type
Comment
Return
EventCallbackCmpEventMgr_Interfaces.RTS_IEC_RESULTInput
pEventParamPOINTER TO CmpEventMgr_Interfaces.EventParam
Pointer to the event parameters, see Struct EventParam