IPaintSelectionInElement.FrameSize (PROP)
PROPERTY FrameSize : INT
If the frame size < 0 the default frame size is used. The fame size is used to increase the layer size of the selection layer
IPaintSelectionInElement.FrameSize (PROP)PROPERTY FrameSize : INT
If the frame size < 0 the default frame size is used. The fame size is used to increase the layer size of the selection layer