VisuFbFileTransferManager.RequestStreamingPlcToVisu (METH)
METHOD RequestStreamingPlcToVisu
- InOut:
Scope
Name
Type
Comment
Input
itfVisuStreamReaderThis must be an instance of IVisuStreamReader, that provides the data sent from the plc to the visualization
pxOptTransferActivePOINTER TO BOOL
Point to an optionally configured BOOL variable, that will indicate, whether currently the streaming is active
pxOptTransferSuccessfulPOINTER TO BOOL
Point to an optionally configured BOOL variable, that will indicate, whether the last streaming was successful or not
pxOptErrorCodePOINTER TO Visu_AllNumericTypesUnion
Point to an optionally configured numeric variable, that will receive the error code
tcOptErrorCodeType__SYSTEM.TYPE_CLASSContains the type of the variable pxOptErrorCode points to
xDoNotUsePropertyInfoBOOLThis flag is TRUE, when called from the generated code of the visualization, where the compiler define VISU_USEPROPERTYINFO might be defined.
dwControlFlagsDWORD