VisuFbDateTimeNamesLocalizer.GetDayLong (METH)
METHOD GetDayLong : CharBufferPtr
returns the localized text of the day as whole name. If no localization exists, a defaulttext (textid) should be returned. The stored value, the returnpointer is set to, will be overridden by any next call of one of the Get-methods of this functionblock. Therefore, the result should be used at once. The pointer should not be stored.
- InOut:
Scope
Name
Type
Comment
Return
GetDayLongCharBufferPtrInput
uiDayOfWeekUINTDay of Week: 1: Monday, 2: Tuesday,.. 7: Sunday