ConnectorFlagController
- Code example for setting:
myCf: IoDrvUtility.ConnectorFlagController; // Define in FB of IoDrv /// In UpdateConfiguration: myCf.Init(m_pConnector, nCount, TRUE); // Last parameter is _xSetChildren /// Somewhere else (UpdateConfiguration, IoDrvStartBusCycle, AsyncTask, ...): myCf.State := IoDrvUtility.ConnectorState.NO_DRIVER_FOUND; myCf.DiagnosticAvailable := FALSE; myCf.DemolicenseActive := FALSE;
- Code example for reading:
myCf: ConnectorFlagController; // Define in FB of IoDrv /// In UpdateConfiguration: myCf.Init(m_pConnector, 0, FALSE); // Last parameter is _xSetChildren, nCount dosen´t matter -> no Children are set /// Somewhere in your code, e.g. PLG_PRG if( myCf.State = IoDrvUtility.ConnectorState.RUNNING) THEN ; END_IF if( myCf.DiagnosticAvailable ) THEN ; END_IF if( myCf.DemolicenseActive ) THEN ; END_IF
This lib/folder/project simplifies the use of the ConnectorFlags, which are processed in 4 different locations:
In AutomationPlatform\Implementation\Sources and Projects\DefaultNavigators\Common.cs are set the pictures in the tree and the color for the text in the tree:
In AutomationPlatform\Implementation\Sources and Projects\DeviceEditor\StatusControl.cs is set the status text over “_tbStatus.Text”:
In AutomationPlatform\Implementation\Sources and Projects\DeviceEditor\IOMappingEditorPage.cs in UpdateModuleStatus is set a warning in the I/O Mapping tab, if an errorflag is set:
In the Device Diagnosis (Enduser can wait until the bus is in “running”-state to start his programm or can react, if the bus has crashed) :
DED can be activated over the PLC settings:
The following table shows the result of the 4 different locations to the 3 changeable properties (ConnectorFlagController.State, ConnectorFlagController.DiagnosticAvailable, ConnectorFlagController.DemolicenseActive) in the version 3.5 SP9:
In the version 3.5 SP8 and before it is:
EnumsFunctionBlocksConnectorFlagController(FB)ConnectorFlagController.AutoFlush(PROP)ConnectorFlagController.AutoSetErrorClearedFlag(PROP)ConnectorFlagController.Connector(PROP)ConnectorFlagController.DemolicenseActive(PROP)ConnectorFlagController.DiagProvider(PROP)ConnectorFlagController.DiagnosticAvailable(PROP)ConnectorFlagController.ErrorClearedActive(PROP)ConnectorFlagController.Flush(METH)ConnectorFlagController.Init(METH)ConnectorFlagController.SetChildren(PROP)ConnectorFlagController.SkipDisabledChildConnectors(PROP)ConnectorFlagController.State(PROP)ConnectorFlagController.nCount(PROP)
_ExternalFilesDoku