DatasourcesMgr.GetDatasource (METH)
METHOD GetDatasource : IDatasources.IDatasource
Returns the datasource representing the given object’s name.
- InOut:
Scope
Name
Type
Comment
Return
GetDatasourceIDatasources.IDatasourceThe datasource object or 0 in case there is none with the given name.
Input
nameSTRINGThe name of the datasource as configured in the according object’s name in the project