DatasourcesMgr.BeginDataConfiguration (METH)
METHOD BeginDataConfiguration : SysTypes.RTS_IEC_RESULT
This method locks the concurrent task for monitoring items and allows subsequent accesses to the configuration of the active. To unlock again afterwards, call EndDataConfiguration .. important:: Before calling methods like UseData or ReleaseData it is necessary to do this syncronisation to prevent undefined behaviour.
- InOut:
Scope
Name
Type
Comment
Return
BeginDataConfigurationSysTypes.RTS_IEC_RESULTReturns a runtime system error code (see CmpErrors.library) or one of |Errors|
Input
xBlockingBOOLThis variable signals the way to do the synchronization. TRUE: the call will be blocking FALSE: the call will be nonblocking and might faile with the error code [Errors.ERR_DS_MULTITASKING_LOCKED|