StateMachine.ShuttingDown (METH)
METHOD ShuttingDown : SysTypes.RTS_IEC_RESULT
This method is called during the shutdown sequence. Implementations can use it to implement the shutdown sequence (like loggint out from the connected device, closing connection resources etc.)
- InOut:
Scope
Name
Type
Comment
Return
ShuttingDownSysTypes.RTS_IEC_RESULTAn error code representing the result of this operation. In case an error happens, an according eror code should be returned. In case the sequence is not yet finished, CmpErrors.Errors.ERR_PENDING should be returned. After a successfull or failed return, the implementation should be in a state where a new connection could be setup using a possible followup call to |IDriverStateMachine.StartConnect|.