StateMachine.PollRequestResult (METH)
METHOD PollRequestResult : SysTypes.RTS_IEC_RESULT
Using this method the driver is polled whether the given request is already finshed.
- InOut:
Scope
Name
Type
Comment
Return
PollRequestResultSysTypes.RTS_IEC_RESULTAn error code representing the result of the polling operation. In case the operation is not yet finished, CmpErrors.Errors.ERR_PENDING should be returned. When it finished successfully, CmpErrors.Errors.ERR_OK should be returned. When sending a request failed, an error code should be returned and then the whole connection will be set up again.
Input
requestIDatasources.IDriverRequestThe request object to check for it’s result