Variance (FB)
FUNCTION_BLOCK Variance
This function will update the experimental variance of the mean with respect to the new input parameter \(x_{n}\),
which will be added to a series of data \(x_{n-1},\dots,n_{1}\) (stemming from previous calls).
The variance \(s\) of the data \(x_{n},\dots,x_{1}\) is calculated according to: \(s = \frac{1}{n}\sum_{i=1}^{n}\left(x_{i} - \bar{x}\right)\),
where \(\bar{x}\) is the arithmetic mean of the data.
- InOut:
Scope
Name
Type
Comment
Input
xEnableBOOLReset
lrInputValueLREALNew data \(x_{n}\)
Output
lrVarianceLREALExperimental variance of the mean of \(x_{n},\dots,x_{1}\)