Statistics_LREAL (FB)
FUNCTION_BLOCK Statistics_LREAL
This function block will update the values of minimum, maximum and average with respect to the integral input parameter \(x_{n}\),
which will be added to a set of integral data \(x_{n-1},\dots,n_{1}\) (stemming from previous calls).
The arithmetic mean \(\bar{x}\) of the values \(x_{n},\dots,x_{1}\) is calculated by:
\[\bar{x} = \frac{1}{n}\sum_{i=1}^{n}x_{i}\]
- InOut:
Scope
Name
Type
Initial
Comment
Input
xEnableBOOLReset
lrInputLREALNew data \(x_{n}\)
Output
lrMinLREALLREAL#1E+80
Minimum of set \(x_{n},\dots,x_{1}\)
lrMaxLREALLREAL#-1E+80
Maximum of set \(x_{n},\dots,x_{1}\)
lrAverageLREALArithmetic mean of data \(x_{n},\dots,x_{1}\)
xOverrunBOOLTRUE: In case of overflowThe module will compensate this by a minor weighting of the old data leading to inaccuracy of the result