Statistics_DINT (FB)

FUNCTION_BLOCK Statistics_DINT

This function block will update the values of minimum, maximum and average with respect to the integral input parameter \(x_{n}\), which will be added to a set of integral data \(x_{n-1},\dots,x_{1}\) (stemming from previous calls).

\[\left \lfloor \frac{\sum_{i=1}^{n}x_{i}+\left \lfloor \frac{n}{2} \right \rfloor}{n} \right \rfloor\]

Note

Pay attention, that the returned average is of type DINT. In contrast to the arithmetic mean the result will be rounded.

InOut:

Scope

Name

Type

Initial

Comment

Input

xEnable

BOOL

Reset

diInput

DINT

New data \(x_{n}\)

Output

diMin

DINT

16#7FFFFFFF

Minimum of set \(x_{n},\dots,x_{1}\)

diMax

DINT

DWORD_TO_DINT(16#80000000)

Maximum of set \(x_{n},\dots,x_{1}\)

diAverage

DINT

Rounded avarage of data \(x_{n},\dots,x_{1}\)

xOverrun

BOOL

TRUE: In case of overflow
The module will compensate this by a minor weighting of the old data leading to inaccuracy of the result