IDevice2.CheckCurrentSupportedCommunicationState (METH)
METHOD CheckCurrentSupportedCommunicationState : BOOL
This method checks if a specific DEVICE_TRANSITION_STATE can be processed in the current state.
Note
Use IDevice2.CheckSupportedCommunicationState to check which DEVICE_TRANSITION_STATE is supported in general.
- InOut:
Scope
Name
Type
Comment
Return
CheckCurrentSupportedCommunicationStateBOOLTrue if node supports the requested DEVICE_TRANSITION_STATE in the current state.
Input
eRequestedStateThe communication state to be checked.