GetIDeviceInstByIoAddr (FB)
FUNCTION_BLOCK GetIDeviceInstByIoAddr EXTENDS ETrigA IMPLEMENTS ICmpEventCallback
This function block returns the associated IDevice object for a specific I/O address.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError,iError) are present at the outputs for exactly one cycle.ETrigA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigA
Output
xDoneBOOLTRUE: Action successfully completedETrigA
xBusyBOOLTRUE: Function block activeETrigA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigA
xAbortedBOOLTRUE: Action aborted by userETrigA
Input
dwAddressDWORDAddress of the I/O Channel (e.g.
ADR(%QB0))dwBitOffsetDWORDBit Offset starting at 0; must be set for bitchannels
Output
itfDeviceIDevice instance of the device, the I/O channel belongs to.