Reconfigure (FB)
FUNCTION_BLOCK Reconfigure EXTENDS ETrig
This function block reads and applies the whole configuration of the corresponding device and all subdevices.
After Reconfiguring all changed configuration values (Enable flag, Parameter changes, …) take effect.
If device doesn’t support reconfiguring eError returns ERROR.NOT_SUPPORTED.
Example
Following example code disables a slave device beneath a fieldbus master.
PROGRAM PLC_PRG
VAR
iState : INT := 0;
reconfig : DED.Reconfigure;
END_VAR
CASE iState OF
0: //Disable slave device: Slave1 (= name in device tree)
Slave1.Enable := FALSE;
iState := 1;
1: //start reconfiguring of fieldbus master
reconfig(xExecute := TRUE, itfNode := Master);
IF reconfig.xDone THEN
iState := 3;
ELSIF reconfig.xError THEN
iState := 2;
END_IF
2: //reconfiguring error
//TODO: Add code here
reconfig(xExecute := FALSE);
3: //reconfiguring successful ==> slave disabled
//TODO: Add code here
reconfig(xExecute := FALSE);
END_CASE
Note
This feature may not be supported by all fieldbus drivers.
eError will return ERROR.NOT_SUPPORTED if not supported.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrig
Output
xDoneBOOLTRUE: Action successfully completedETrig
xBusyBOOLTRUE: Function block activeETrig
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrig
Input
itfNodeThe node to be reconfigured.
Output
eErroroperation error code