SDO_WRITE_DATA (FB)
FUNCTION_BLOCK SDO_WRITE_DATA EXTENDS CiA405Base
This function block is used for writing a specific object in object dictionary of a DEVICE.
If DATA was written without error CONFIRM becomes TRUE.
DATA has to be in Little Endian byte order.
If an error occurs ERROR becomes unequal 0. In case of a SDO abort ERROR is set to CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_OTHER_ERROR
and ERRORINFO contains the associated abort code (in Little endian) as defined by CiA 301.
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
NETWORKUSINT1
CAN network number the function block should operate on. Note: It is not the same like the network number in CANBus configurator. The CiA405
NETWORKis calculated by NetID + 1. Example: 1 = CAN0, 2 = CAN1, 3 = CAN2, …CiA405Base
ENABLEBOOLFALSE
Enables the function block on rising edge. Aborts operation on falling edge.
CiA405Base
TIMEOUTUDINT0
Timeout in ms; 0 means no timeout
CiA405Base
Output
CONFIRMBOOLFALSE
TRUE: function block finished without errorCiA405Base
ERRORCANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR
Error code: see CANOPEN_KERNEL_ERROR for further details
CiA405Base
Input
DEVICENodeID of destination device; 0 means local device (= CANopenManager)
CHANNELUSINT1
SDO channel: 0: use any free channel; 1..n: specific channel
INDEXWORDIndex of object
SUBINDEXBYTESubIndex of object
MODESDO_MODE.AUTO
specifies the SDO Mode to be used
DATAPOINTER TO BYTE
pointer to data which should be written (data has to be in little endian byte order)
DATALENGTHUDINTlength of data in bytes
Output
ERRORINFOcontains abort code in little endian in case of
ERRORis CANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_OTHER_ERROR