RECV_EMCY_DEV (FB)
FUNCTION_BLOCK RECV_EMCY_DEV EXTENDS CiA405Base
Function block checks if an emergency object has been received from NodeID specified by input DEVICE.
If the function block has finished its action without any error, output CONFIRM is changed to
TRUE and ERROR to 0.
Member EMCY_ERROR_CODE of output ERRORINFO is unequal zero if an EMCY is pending.
If EMCY_ERROR_CODE equals zero no EMCY is currently pending.
Note
A received emergency is not cleared and it is delivered with each call of the function block until the device sends an emergency reset.
If an error occurred while checking for an emergency, CONFIRM is set to FALSE and ERROR is set to
the corresponding error value.
- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
NETWORKUSINT1
CAN network number the function block should operate on. Note: It is not the same like the network number in CANBus configurator. The CiA405
NETWORKis calculated by NetID + 1. Example: 1 = CAN0, 2 = CAN1, 3 = CAN2, …CiA405Base
ENABLEBOOLFALSE
Enables the function block on rising edge. Aborts operation on falling edge.
CiA405Base
TIMEOUTUDINT0
Timeout in ms; 0 means no timeout
CiA405Base
Output
CONFIRMBOOLFALSE
TRUE: function block finished without errorCiA405Base
ERRORCANOPEN_KERNEL_ERROR.CANOPEN_KERNEL_NO_ERROR
Error code: see CANOPEN_KERNEL_ERROR for further details
CiA405Base
Input
DEVICE0
NodeID of device
Output
ERRORINFOEMCY information; if member
EMCY_ERROR_CODEis zero, no EMCY is pending.