TRANSITION_STATE (ENUM)
TYPE TRANSITION_STATE :
Describes the NMT state transitions for function block GET_STATE.
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
START_REMOTE_NODE
16#5
Enter DEVICE_STATE.OPERATIONAL
STOP_REMOTE_NODE
16#4
Enter DEVICE_STATE.STOPPED
ENTER_PRE_OPERATIONAL
16#7F
RESET_NODE
16#6
Reset node
RESET_COMMUNICATION
16#7
Reset communication
ALL_EXCEPT_NMT_AND_SENDER
16#800
A flag for using in combination with another
TRANSITION_STATE(logical OR). Must be used if NMT command should be addressed to all devices (``DEVICE``=0) but not to the NMT sender and NMT master (= CANopenManager).