SDO_READ (STRUCT)
TYPE SDO_READ : STRUCT
Structure is only compatible with 3.5 SP7 runtime or newer
- InOut:
Name
Type
Comment
usiNodeIdUSINTusiChannelUSINTuiIndexUINTusiSubIndexUSINTxUseSpecificTimeoutBOOLTRUE: ctTimeout will be used; ELSE: default timeout
xBlockTransferBOOLusiPSTUSINTProtocol Switch Threshold in bytes (only for block transfer)
uiStateUINTxLegacyCRCBOOLFALSE: Use default CANopen CRC for block transfer; TRUE: Use legacy CRC (used before 3.5 SP10).
xDummyBOOLudiSizeUDINTpDataCAA.PVOIDudiAbortCodeUDINTctTimeoutCAA.COUNTTimeout in us