BACnetObjectBase.SetBACnetAccumulatorRecordProperty (METH)
METHOD SetBACnetAccumulatorRecordProperty
Sets the BACnet-Accumulator-Record of the specified Property (propID) of this BACnet-Object using a IEC_BACNET_ACCUMULATOR_RECORD struct. The used functions are no client, meaning, that the access of the property is not restricted by write or read access restrictions.
- InOut:
Scope
Name
Type
Comment
Input
propIDCmpBACnet.IEC_BACNET_PROPERTY_IDThe ID of the property to set.
accRecCmpBACnet.IEC_BACNET_ACCUMULATOR_RECORDThe accumulator record to set.